AXIS#.IL.COGCOMP.TEACH.DEC

Description

Sets the deceleration used during the Cogging Compensation teach.

Versions

Action Version Notes
Implemented 02-08-00-000

General Information

Type

Read/Write

Units

Rotary: RPM/s, RPS/s, deg/s2, (custom units)/s2, rad/s2

See Acceleration Units for details.

Range

Depends on units. See Acceleration Range for details.

Default Value 30,000 rpm/s

Data Type

Float
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
AXIS1.IL.COGCOMP.TEACH.DEC

500ah

20h

Unsigned32

Acceleration

-

Read/Write

No

AXIS2.IL.COGTABLE.TEACH.DEC

510ah

20h

Unsigned32

Acceleration

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.IL.COGCOMP.TEACH.DEC

5851

16DB

Unsigned32

Read/Write

Acceleration

AXIS2.IL.COGCOMP.TEACH.DEC

71387

116D

Unsigned32

Read/Write

Acceleration

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.COGCOMP.TEACH.DEC

5851

Float

Read/Write

Acceleration